Base Module.Configuration Registers.Print
June 21, 2021

Base Module - SBp.0101.01 - Configuration Registers

Index: all SLATE modules Version: June 21, 2021

0101      Base Module - SBp.0101.01 - Configuration Registers
Open printable version | Printing help




< > Resize  |  Click below to view:
1 Module number - Module Setup 6 Alert display level - Module Setup 7 Install date - Module Setup 16 Module short name - Module Setup 17 Module name - Module Setup 100 RS485 protocol - Communication Setup 101 RS-485 baud rate - Communication Setup 102 RS-485 parity - Communication Setup 103 Modbus RS-485 slave address - Communication Setup 104 Modbus/TCP configuration - Communication Setup 105 Modbus/TCP port - Communication Setup 106 BACnet/MSTP MAC address - Communication Setup 107 BACnet device object instance - Communication Setup 108 BACnet Ethernet configuration - Communication Setup 109 BACnet device name - Communication Setup 110 BACnet IP port - Communication Setup 111 BACnet DCC/RD password - Communication Setup 112 BACnet BBMD Name/IP address - Communication Setup 113 BACnet BBMD UDP port - Communication Setup 114 BACnet minimum UDP local port - Communication Setup 115 BACnet maximum UDP local port - Communication Setup 116 BACnet max info frames - Communication Setup 117 BACnet max master - Communication Setup 118 Ethernet IP address source - Communication Setup 119 Ethernet IP address - Communication Setup 120 Ethernet subnet mask - Communication Setup 121 Ethernet router address - Communication Setup 122 Ethernet DNS address - Communication Setup 125 Date/time format - System Setup 126 Daylight savings setting - System Setup 127 Time zone - System Setup 130 SLATE device name - System Setup 131 Installation notes - System Setup 132 Display sleep delay time - System Setup 133 Login pass code - System Setup 134 Login timeout - System Setup 136 Temperature display format - System Setup 139 BACnet re-registration interval - Communication Setup 300 BACnet bind 1 setup - BACnet Binding 303 BACnet bind 2 setup - BACnet Binding 306 BACnet bind 3 setup - BACnet Binding 309 BACnet bind 4 setup - BACnet Binding 312 BACnet bind 5 setup - BACnet Binding 315 BACnet bind 6 setup - BACnet Binding 318 BACnet bind 7 setup - BACnet Binding 321 BACnet bind 8 setup - BACnet Binding 324 BACnet bind 9 setup - BACnet Binding 327 BACnet bind 10 setup - BACnet Binding 330 BACnet bind 11 setup - BACnet Binding 333 BACnet bind 12 setup - BACnet Binding 336 BACnet bind 13 setup - BACnet Binding 339 BACnet bind 14 setup - BACnet Binding 342 BACnet bind 15 setup - BACnet Binding 345 BACnet bind 16 setup - BACnet Binding 348 BACnet bind 17 setup - BACnet Binding 351 BACnet bind 18 setup - BACnet Binding 354 BACnet bind 19 setup - BACnet Binding 357 BACnet bind 20 setup - BACnet Binding 410 Aux voltage source - Module Setup 411 Aux voltage non-volatile setting - Module Setup 412 Aux current limit setting - Module Setup 417 Light detector sensitivity - Module Setup 419 Backlight brightness - Module Setup

1  Module number Category: Module Setup
  Units;
DataType:
Max:
Default Value:
Min:
VAL-uint16
U16

255

Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
2
Yes
Yes - Configuration data
Yes - Safety data
No - Field setup only
  Description: Assigned module number


6  Alert display level Category: Module Setup
  Units;
DataType:
Max:
Default Value:
Min:
VAL-ubyte
U8

0

Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
1
Yes
Yes - Configuration data
No
Yes - Can set up in AX
  Description: Enable/disable alert output (0=Disable, >0=Alert context level)


7  Install date Category: Module Setup
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String



Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
20
Yes
Yes - Configuration data
No
Yes - Can set up in AX
  Description: Date when this module was installed in this system


16  Module short name Category: Module Setup
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String

Base

Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
10
Yes
Yes - Configuration data
No
No - Field setup only
  Description: Short module name for Base display use


17  Module name Category: Module Setup
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String

Base

Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
60
Yes
Yes - Configuration data
No
No - Field setup only
  Description: Full module name for display use


100  RS485 protocol Category: Communication Setup
  Units;
DataType:
Max:
Default Value:
Min:
VAL-uint16
EnumSingle
1
1
3
Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
2
Yes
Yes - Configuration data
No
No - Field setup only
  Description: Communication protocol for RS-485 port.
1 None No communication protocol
2 Modbus Modbus RTU slave
3 BACnet MS/TP BACnet MS/TP slave


101  RS-485 baud rate Category: Communication Setup
  Units;
DataType:
Max:
Default Value:
Min:
VAL-uint16
EnumSingle
1
4
7
Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
2
Yes
Yes - Configuration data
No
No - Field setup only
  Description: Sets the speed of the external RS-485 port.
1 None RS-485 port speed is unconfigured
2 9600 The baud rate to 9600 bits per second
3 19200 The baud rate to 19200 bits per second
4 38400 The baud rate to 38400 bits per second
5 57600 The baud rate to 57600 bits per second
6 76800 The baud rate to 76800 bits per second
7 115200 The baud rate to 115200 bits per second


102  RS-485 parity Category: Communication Setup
  Units;
DataType:
Max:
Default Value:
Min:
VAL-uint16
EnumSingle
1
1
3
Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
2
Yes
Yes - Configuration data
No
No - Field setup only
  Description: Determines if parity is used, and if so, whether it is odd or even.
1 None No parity requirement for RS-485 communication
2 Odd RS-485 communication is done with Odd parity
3 Even RS-485 communication is done with Even parity


103  Modbus RS-485 slave address Category: Communication Setup
  Units;
DataType:
Max:
Default Value:
Min:
VAL-ubyte
U8
1
1
255
Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
1
Yes
Yes - Configuration data
No
No - Field setup only
  Description: Address of the Kettos base as a Modbus slave for the external RS-485 bus.


104  Modbus/TCP configuration Category: Communication Setup
  Units;
DataType:
Max:
Default Value:
Min:
VAL-uint16
EnumSingle

1

Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
2
Yes
Yes - Configuration data
No
No - Field setup only
  Description: Configure Modbus via Ethernet TCP.
1 None The ethernet interface is not used for Modbus communication
2 Modbus/TCP Modbus/TCP is enabled for the ethernet interface


105  Modbus/TCP port Category: Communication Setup
  Units;
DataType:
Max:
Default Value:
Min:
VAL-uint16
U16
0
502
65535
Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
2
Yes
Yes - Configuration data
No
No - Field setup only
  Description: Default port for Modbus/TCP communication.


106  BACnet/MSTP MAC address Category: Communication Setup
  Units;
DataType:
Max:
Default Value:
Min:
VAL-uint16
U16
0
1
254
Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
2
Yes
Yes - Configuration data
No
No - Field setup only
  Description: Address for BACnet communication via the RS-485 based MS/TP protocol.


107  BACnet device object instance Category: Communication Setup
  Units;
DataType:
Max:
Default Value:
Min:
xAX VAL-uint32
U32
0
0
4194302
Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
4
Yes
Yes - Configuration data
No
No - Field setup only
  Description: Instance number of the BACnet Device Object. Every device in a BACnet network must have a unique Instance number for it's Device Object.


108  BACnet Ethernet configuration Category: Communication Setup
  Units;
DataType:
Max:
Default Value:
Min:
VAL-uint16
EnumSingle

1

Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
2
Yes
Yes - Configuration data
No
No - Field setup only
  Description: Type of BACnet interface used on Ethernet port connection. Selection must be "None" if RS-485 port is configured for BACnet MS/TP.
1 None The ethernet interface is not used for BACnet communication. Note that this must be set if the RS-485 port is used for BACnet MS/TP.
2 BACnet/Ethernet BACnet/Ethernet is enabled on the ethernet interface
3 Plain BACnet/IP Plain BACnet/IP is enabled on the ethernet interface
4 Register as foreign device


109  BACnet device name Category: Communication Setup
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String



Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
30
Yes
Yes - Configuration data
No
No - Field setup only
  Description: The same BACnet device name is used by both the RS-485/MSTP BACnet and the ethernet BACnet/IP, even though they may have different object instances if they are different BACnet networks. The device name is required to be unique in a BACnet network.


110  BACnet IP port Category: Communication Setup
  Units;
DataType:
Max:
Default Value:
Min:
VAL-uint16
U16
0
47808
65535
Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
2
Yes
Yes - Configuration data
No
No - Field setup only
  Description: Default port for BACnet UDP communication. Normal port setting is hexadecimal 0xBAC0 (47808 decimal).


111  BACnet DCC/RD password Category: Communication Setup
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String



Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
20
Yes
Yes - Configuration data
No
No - Field setup only
  Description: Password required for the DeviceCommunicationControl and ReinitializeDevice services.


112  BACnet BBMD Name/IP address Category: Communication Setup
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String



Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
60
Yes
Yes - Configuration data
No
No - Field setup only
  Description: Name or IP address for BACnet/IP Broadcast Management Device (BBMD) routing.


113  BACnet BBMD UDP port Category: Communication Setup
  Units;
DataType:
Max:
Default Value:
Min:
VAL-uint16
U16
0
47808
65535
Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
2
Yes
Yes - Configuration data
No
No - Field setup only
  Description: UDP port for BACnet/IP Broadcast Management Device (BBMD) routing.


114  BACnet minimum UDP local port Category: Communication Setup
  Units;
DataType:
Max:
Default Value:
Min:
VAL-uint16
U16
0
50000
65535
Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
2
Yes
Yes - Configuration data
No
No - Field setup only
  Description: Minimum UDP port for BACnet interface. When registered as a foreign device, SLATE chooses an unused local UDP port in the range between min and max for receiving messages. Any other BACnet/IP UDP ports on the same subnet must be outside of this range.


115  BACnet maximum UDP local port Category: Communication Setup
  Units;
DataType:
Max:
Default Value:
Min:
VAL-uint16
U16
0
50099
65535
Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
2
Yes
Yes - Configuration data
No
No - Field setup only
  Description: Maximum UDP port for BACnet interface. When registered as a foreign device, SLATE chooses an unused local UDP port in the range between min and max for receiving messages. Any other BACnet/IP UDP ports on the same subnet must be outside of this range.


116  BACnet max info frames Category: Communication Setup
  Units;
DataType:
Max:
Default Value:
Min:
VAL-uint16
U16
1
1
65535
Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
2
Yes
Yes - Configuration data
No
No - Field setup only
  Description: Maximum number of information frames that are allowed before the device should give up control of the BACnet network.


117  BACnet max master Category: Communication Setup
  Units;
DataType:
Max:
Default Value:
Min:
VAL-uint16
U16
1
127
127
Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
2
Yes
Yes - Configuration data
No
No - Field setup only
  Description: Maximum number of master devices on the BACnet network.


118  Ethernet IP address source Category: Communication Setup
  Units;
DataType:
Max:
Default Value:
Min:
VAL-uint16
EnumSingle

2

Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
2
Yes
Yes - Configuration data
No
No - Field setup only
  Description: Use dynamic or static IP addressing.
1 DHCP IP address Dynamic address assigned by DHCP server
2 Static IP address Static IP address


119  Ethernet IP address Category: Communication Setup
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String

192.168.92.10

Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
16
Yes
Yes - Configuration data
No
No - Field setup only
  Description: IP address used by Ethernet port when static addressing is used. Ignored when DHCP is enabled.


120  Ethernet subnet mask Category: Communication Setup
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String

255.255.255.0

Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
16
Yes
Yes - Configuration data
No
No - Field setup only
  Description: Ethernet subnet mask when static IP assignment is used. Ignored if DHCP is enabled.


121  Ethernet router address Category: Communication Setup
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String

192.168.92.1

Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
16
Yes
Yes - Configuration data
No
No - Field setup only
  Description: Ethernet IP address of the subnet's router when static IP addressing is used. Ignored if DHCP is enabled.


122  Ethernet DNS address Category: Communication Setup
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String

192.168.92.1

Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
16
Yes
Yes - Configuration data
No
No - Field setup only
  Description: Ethernet address of the Domain Name Server, if any, when static IP addressing is used. Empty value indicates that no DNS is used. Ignored if DHCP is enabled.


125  Date/time format Category: System Setup
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String

8601; 12; ns

Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
20
Yes
Yes - Configuration data
No
No - Field setup only
  Description: Select the format for display of date and time. Four strings can be provided separated by space and/or semicolon. The first may be ymd, mdy, dmy, or 8601 (e.g. for February 2 2014 these show, respectively 2014/2/4, 2/4/2014, and 2014-02-04 (the last is the ISO 8601 standard form). The second string can be 24 or 12 for 24 hour time or 12 hour time with am/pm. The third can be s or ns to include or omit seconds. The fourth is ddd or dayname or empty to include the dayname as a 3 letter abbreviation a full word, or omit the dayname. If any of the strings is empty then the defaults are: 8601, 12, ns, and omit the dayname.


126  Daylight savings setting Category: System Setup
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String

2,3;1,11

Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
12
Yes
Yes - Configuration data
No
No - Field setup only
  Description: Determine when daylight savings time transitions will occur. 2:00 AM on a Sunday is assumed. The value is two pairs of values separated by space or a semicolon. Each value is a numeral 1 through 4 corresponding to the 1st through the 4th Sunday or the letter L corresponding to the last Sunday, then a comma, then a month number. E.g. the current USA standard is thus 2,3;1,11 ( 2nd Sunday in March, 1st Sunday in November). An empty value indicates no DST changes are to be made.


127  Time zone Category: System Setup
  Units;
DataType:
Max:
Default Value:
Min:
VAL-float
F32

0

Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
4
Yes
Yes - Configuration data
No
No - Field setup only
  Description: Time zone of this installation. This number, between -12 and +12, corresponds to the UTC offset from GMT. GMT is 0, Eastern is -5, Central is -6, Mountain is -7, Pacific is -8, etc. Fractional values may be used, e.g. India should be 5.5.


130  SLATE device name Category: System Setup
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
UTF8



Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
80
Yes
Yes - Configuration data
No
Yes - Can set up in AX
  Description: Name assigned to entire system. This name can use any character encoding supported by UTF-8 format value.


131  Installation notes Category: System Setup
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String



Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
150
Yes
Yes - Configuration data
No
Yes - Can set up in AX
  Description: Notes regarding the system installation.


132  Display sleep delay time Category: System Setup
  Units;
DataType:
Max:
Default Value:
Min:
minute
U16
0
30
1440
Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
72
2
Yes
Yes - Configuration data
No
Yes - Can set up in AX
  Description: Time period of no activity that must elapse before the Base display and the LEDs are turned off to save power and their lifespan. Activity consists of pressing buttons on the Base or any module and also, if enabled, light increases that are significant per the sensitivity setting from the light sensor. A zero value disables the sleep function.


133  Login pass code Category: System Setup
  Units;
DataType:
Max:
Default Value:
Min:
VAL-uint16
U16
0
1111
9999
Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
2
Yes
Yes - Configuration data
No
Yes - Can set up in AX
  Description: Password code that must be entered by the local user at the Base module display to successfully log into the system for priviledged access. Log in remains active while the user continues to interact with the keys on the modules or until the time period specified in the Login timeout parameter expires following the login.


134  Login timeout Category: System Setup
  Units;
DataType:
Max:
Default Value:
Min:
second
U16
300
600
1800
Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
73
2
Yes
Yes - Configuration data
No
Yes - Can set up in AX
  Description: Maximum time period that a successful login lasts without any user interaction before the login status is terminated.


136  Temperature display format Category: System Setup
  Units;
DataType:
Max:
Default Value:
Min:
VAL-uint16
EnumSingle

1

Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
2
Yes
Yes - Configuration data
No
No - Field setup only
  Description: Default display format for temperature in system, Fahrenheit or Celsius.
1 No conversion Display temperature and degrees in it's internal units.
2 Celsius Display temperature and degrees in Celsius format.


139  BACnet re-registration interval Category: Communication Setup
  Units;
DataType:
Max:
Default Value:
Min:
second
U16
0
300
65535
Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
73
2
Yes
Yes - Configuration data
No
No - Field setup only
  Description: Time interval for re-registering this system as a BACnet foreign device.


300  BACnet bind 1 setup Category: BACnet Binding
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String



Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
100
Yes
Yes - Configuration data
No
No - Field setup only
  Description: For value format see the SLATE BACnet specification


303  BACnet bind 2 setup Category: BACnet Binding
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String



Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
100
Yes
Yes - Configuration data
No
No - Field setup only
  Description: For value format see the SLATE BACnet specification


306  BACnet bind 3 setup Category: BACnet Binding
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String



Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
100
Yes
Yes - Configuration data
No
No - Field setup only
  Description: For value format see the SLATE BACnet specification


309  BACnet bind 4 setup Category: BACnet Binding
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String



Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
100
Yes
Yes - Configuration data
No
No - Field setup only
  Description: For value format see the SLATE BACnet specification


312  BACnet bind 5 setup Category: BACnet Binding
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String



Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
100
Yes
Yes - Configuration data
No
No - Field setup only
  Description: For value format see the SLATE BACnet specification


315  BACnet bind 6 setup Category: BACnet Binding
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String



Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
100
Yes
Yes - Configuration data
No
No - Field setup only
  Description: For value format see the SLATE BACnet specification


318  BACnet bind 7 setup Category: BACnet Binding
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String



Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
100
Yes
Yes - Configuration data
No
No - Field setup only
  Description: For value format see the SLATE BACnet specification


321  BACnet bind 8 setup Category: BACnet Binding
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String



Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
100
Yes
Yes - Configuration data
No
No - Field setup only
  Description: For value format see the SLATE BACnet specification


324  BACnet bind 9 setup Category: BACnet Binding
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String



Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
100
Yes
Yes - Configuration data
No
No - Field setup only
  Description: For value format see the SLATE BACnet specification


327  BACnet bind 10 setup Category: BACnet Binding
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String



Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
100
Yes
Yes - Configuration data
No
No - Field setup only
  Description: For value format see the SLATE BACnet specification


330  BACnet bind 11 setup Category: BACnet Binding
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String



Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
100
Yes
Yes - Configuration data
No
No - Field setup only
  Description: For value format see the SLATE BACnet specification


333  BACnet bind 12 setup Category: BACnet Binding
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String



Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
100
Yes
Yes - Configuration data
No
No - Field setup only
  Description: For value format see the SLATE BACnet specification


336  BACnet bind 13 setup Category: BACnet Binding
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String



Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
100
Yes
Yes - Configuration data
No
No - Field setup only
  Description: For value format see the SLATE BACnet specification


339  BACnet bind 14 setup Category: BACnet Binding
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String



Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
100
Yes
Yes - Configuration data
No
No - Field setup only
  Description: For value format see the SLATE BACnet specification


342  BACnet bind 15 setup Category: BACnet Binding
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String



Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
100
Yes
Yes - Configuration data
No
No - Field setup only
  Description: For value format see the SLATE BACnet specification


345  BACnet bind 16 setup Category: BACnet Binding
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String



Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
100
Yes
Yes - Configuration data
No
No - Field setup only
  Description: For value format see the SLATE BACnet specification


348  BACnet bind 17 setup Category: BACnet Binding
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String



Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
100
Yes
Yes - Configuration data
No
No - Field setup only
  Description: For value format see the SLATE BACnet specification


351  BACnet bind 18 setup Category: BACnet Binding
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String



Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
100
Yes
Yes - Configuration data
No
No - Field setup only
  Description: For value format see the SLATE BACnet specification


354  BACnet bind 19 setup Category: BACnet Binding
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String



Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
100
Yes
Yes - Configuration data
No
No - Field setup only
  Description: For value format see the SLATE BACnet specification


357  BACnet bind 20 setup Category: BACnet Binding
  Units;
DataType:
Max:
Default Value:
Min:
xAX string
String



Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
100
Yes
Yes - Configuration data
No
No - Field setup only
  Description: For value format see the SLATE BACnet specification


410  Aux voltage source Category: Module Setup
  Units;
DataType:
Max:
Default Value:
Min:
VAL-uint16
EnumSingle

1

Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
2
Yes
Yes - Configuration data
No
Yes - Can set up in AX
  Description: Determines the source of the voltage setting for the auxillary voltage output.
1 Non-volatile configuration register A non-volatile configuration register determines the Aux voltage output value. Dynamic control is disabled.
2 Dynamic control register Dynamic control by a RAM based register is enabled. The configuration register is ignored.


411  Aux voltage non-volatile setting Category: Module Setup
  Units;
DataType:
Max:
Default Value:
Min:
volt
F32
3.3
3.3
24.0
Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
5
4
Yes
Yes - Configuration data
No
Yes - Can set up in AX
  Description: Voltage output on the Aux voltage connector on the Base module, when it is configured for control by this parameter.


412  Aux current limit setting Category: Module Setup
  Units;
DataType:
Max:
Default Value:
Min:
milliampere
F32
10
250
250
Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
2
4
Yes
Yes - Configuration data
No
Yes - Can set up in AX
  Description: Maximum current to be provided by the Aux voltage supply on the Base module.


417  Light detector sensitivity Category: Module Setup
  Units;
DataType:
Max:
Default Value:
Min:
VAL-ubyte
U8
0
0
10
Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
1
Yes
Yes - Configuration data
No
Yes - Can set up in AX
  Description: Sensitivity of the light sensor to detect enough environmental light change to denote a wake-up or sleep event. A zero value turns off the light detector, otherwise, when light has been low for a while and then increases, this causes the display and LED exit their sleep mode, lighting up all of the displays. This parameter sets the sensitivity of the sensor to the amount and rate of increase where 1 is minimum sensitivity (a significant change is needed over a short time) and 10 is maximum (a lesser change is needed and it may occur over a longer time).


419  Backlight brightness Category: Module Setup
  Units;
DataType:
Max:
Default Value:
Min:
VAL-ubyte
U8
1
5
10
Units Code:
Size:
Writable:
Permanent:
Verified:
DesignSetup:
256
1
Yes
Yes - Configuration data
No
Yes - Can set up in AX
  Description: Sets the brightness of the backlight in the Base module display as a value from 1 (minimum) to 10 (maximum).