SLATE™ Brochures
download SLATE Brochure (English) >
download SLATE Brochure (Spanish) >
download SLATE Brochure (Portuguese) >
download SLATE Brochure (Chinese) >
download SLATE Brochure (French) >
SLATE™ Tools
Slate AX Tools
New! SLATE Tool 3.41_20827 Full Installation Program for Niagara N4
Requires a purchase of a new N4 license, AX 3.8.38 licenses will not work.
Full Installation setup version 3.41 for Niagara N4 platform with Web Editor Tools. This release includes ret fixes to known issues, a migration tool to migrate Niagara 3.8.38 stations, user application libraries and web editor projects to the N4 platform. Included are all modifications and new and improved widgets (web editor 1.2.38) that were implemented for the 2.23/2.41 SLATETool. Refer to the included PDF documents for additional information.
download >
New! SLATE Tool 3.41_20827 Update Installation Program for Niagara N4
Update Installation setup version 3.41 AX and Web Editor Tools. This install is used when the Niagara N4 is already installed.
Included are all modifications and new and improved widgets (web editor 1.2.38) that were implemented for the 2.23/2.41 SLATETool. Refer to the included PDF documents for additional information.
download >
New! SLATE Tool 2.41_20825 Update Installation Program
Update Installation setup version 2.41 AX and Web Editor Tools. This version is for customers that have Niagara 3.8.38 already installed.
This build fixes BACnet duplicate object ID. It also incudes previous fixes which include the following - Fixed several known issues and includes improvements on Modbus resequencing. The latest web editor 1.2.38 includes several new widgets and improvements on existing widgets.
download >
SLATE Tool 2.19 Update Installation Program
Update Installation setup version 2.19 AX and Web Editor Tools. This version is for users that have 2.19 installed and need to run the update due to program corruption. You will not be able to share exported wiresheets with N4 users and this version does not have the latest web editor. It is suggested to upgrade to SlateTool 2.41 to get the latest updates
download >
SlateTool v2.19 Release Notes
Includes SlateTool Release notes, Web Editor v1.2.8 release notes and Web editor instruction manual. These documents are also included with the SlateTool 2.19 Full and Update installations above.
download >
Firmware Updates and Service Packs
New! Fuel Air Fault 37 Service Pack
The Fuel Air Fault 37 service pack (3.33.20230.01.ssp) is intended for Slate systems with firmware revisions 3.20, or greater, that include a SLATE Fuel Air Ratio module (R8001C6001) and one or more Slate Low Torque Actuators (LTA).
download >
New! Slate 3.33 Firmware Update
Includes the Application and Module service packs, readme file, release notes instructions to bootload the FBE and module firmware and the module register information. Module firmware files for hardware rev 67 for the Analog, Limit and Fuel Air modules are included in the module service pack. This download also includes the Export and Import Configurations V1.0 service pack to help back up a 3.20 system before upgrading to FW3.33. Please read the application note for details .
download >
New! Slate 3.33 Firmware Release Notes
Slate 3.33 Release Notes describes the new features added with this release. The release notes are also included in the Firmware 3.33 download above
download >
New! Export and Import Configurations V1.0 service pack
The “Export and Import Configurations V1.0" service pack is intended for firmware revisions 3.20 and 3.33. When installed this service pack allows the user to do a quick backup and restore for 3.20 systems and a full backup and restore for 3.33 systems. Refer to the application note included for more details.
download >
Slate 3.20 Firmware Update
Includes the Application and Module service packs, readme file, release notes and instructions to bootload the FBE and module firmware. Please read carefully and backup your Slate system configuration before proceeding. Also includes module firmware files for hardware rev 67 for the Analog, Limit and Fuel Air modules
download >
Slate 3.20 Firmware Release Notes
Slate 3.20 Release Notes describes the new features added with this release. The release notes are also included in the Firmware download above
download >
ModbusTCP Service Pack
Service pack for firmware version 3.10 to address ModbusTCP applications with multi-client polling. Under certain conditions resources are not released properly which could result in the inability to communicate via ModbusTCP with a Slate device.
download >
Chrome SSL Compatibility
This service pack is only needed for firmware version 3.10 or older when the user installs the Slate certificate for secure browsing of Slate web pages. Chrome versions 58+ required an additional field to be filled for a valid Slate Certificate.
download >
SLATE Service Pack 2.20
Includes 2.20 firmware service pack with instructions. Also includes module hardware update files with bootloader instructions
download >
New! SLATE Module Register Information FW 3.33
Includes register information up to and including the latest 3.33 firmware release. The module information is also included in Firmware 3.33 download.
download >
SLATE Module Register Information FW 3.20
Includes register information up to and including the latest 3.20 firmware release
download >
Slate Certificates for PC browser
This download includes the certificates to install on a PC to allow a secure connection when browsing the Slate Base. This certificate is valid for Chrome, IE and Edge browsers and Slate Base firmware version 2.20 or newer
download>
Update! SLATE 7800 Emulation Tool
The SLATE 7800 Emulation Tool helps set up a SLATE Burner Control that emulates the behavior of one of the Honeywell 7800 SERIES Burner Controls. Update includes support for 64 bit versions of Microsoft Office/Access
download >
SLATE 3.10 Nuevos Parámetros de Estabilización de la Etapa “Run” en el Burner Control (Spanish)


SLATE™ Canned Programs
Device examples for N3(legacy) or N4 tool
New! Five Stage Ramp Soak with web pages >
New! Five Stage Soak No Ramp Auto Start >
Slate Combined Demo >
Hot Standby Application example >
Convert Time Application - seconds to minutes and hours >
General Daily PV Totalizer - Boiler >
Average Flame Signal during Burner run >
Average Analog Input with manual start/stop >
Temperature - Pressure Application >
Stations (convert to N4 station using the Migration tool)
Four Burner Lead Lag Station. user-SLATE >
SLATE Demo Kit and Station >
Macros and Applications (N3 compatible)
4 to 20 Pressure Range Select >
Alarm On Hold Condition >
Alarm Silencing >
Assured Low Fire Lightoff >
Delta Temp >
Frost Protection >
Outdoor Temperature Reset Macro and Application >
Series 60 and 70 Motor Control Application >
Single Element Feedwater >
Simple Lead Lag >
Temperature/Pressure Control PID & On/Off >
Trim Control Application >
Variable Speed Pump >
Simple Manual Totalizer Application >


SLATE™ Documentation
SLATE Security Manual BR-17-64-US
Best Practices for Cyber Security and Network Configuration Safety
download >
SLATE I&I Documentation
Documentation for Base, Burner Control, Fuel Air, Limit, Analog, Digital, Annunciator, Flame Amplifiers, sub-base modules, Touch Display and SLATE Actuators
download >
SLATE™ Videos
Sales Promo Video coming soon in French
How-to Video


SLATE™ White Papers
New! Base GUI message customization
This document describes how to use Base registers 420 and 421 to display an application specific message on the Base GUI
download paper >
Dual Flame Amplifier Support
Guide to using dual flame amplifiers with Slate firmware 3.10
download paper >
Burner Module Parameters firmware 3.10
SLATE Burner module SW 3.10 release - two new parameters have been added to the configuration
download paper >
Annunciator Configuration
New configuration procedure for the Annunciator Module using Slate Tools 2.06
download paper >
BACnet Peer to Peer Configuration
How to configure SLATE BACnet communication in order to pass data between SLATE systems
download paper >
Import/Export Feature
How to move Slate devices between stations using Slate 2.06 Tools new Import and Export Device feature
download paper >
¡Nuevo! Personalización de mensajes de GUI base (Spanish)
Este documento describe cómo usar los registros base 420 y 421 para mostrar un mensaje específico de la aplicación en la interfaz gráfica de usuario base.
download paper >
Nuevos Parámetros de Estabilización de la Etapa “Run” en el Burner Control 3.10 (Spanish)


SLATE™ Sales Solutions
SLATE Success Stories
Read how SLATE enhances control and efficiency in a variety of applications.
download >
SLATE™ Technical Notes
Base Read/Write Registers
A description of how to use the Base Read/Write registers. There are 5 in firmware rev 3.10 and 10 in revisions 3.20 and 3.33
download >
Registros base de lectura/escritura
Una descripción de cómo utilizar los registros base de lectura/escritura. Hay 5 en el firmware rev 3.10 y 10 en las revisiones 3.20 y 3.33
download >
SLATE™ Remote Training
Slate Online Training
Capacitación online de Slate - Sesiones de noviembre de 2025, Día 1
Sesión del día 1 de noviembre de 2025
download >
Capacitación online de Slate - Sesiones de noviembre de 2025, Día 2
Sesión del día 2 de noviembre de 2025
download >
Capacitación online de Slate - Sesiones de noviembre de 2025, Día 3
Sesión del día 3 de noviembre de 2025
download >
Capacitación online de Slate - Sesiones de noviembre de 2025, Día 4
Sesión del día 4 de noviembre de 2025
download >
Capacitación online de Slate - Sesiones de noviembre de 2025, Día 5
Sesión del día 5 de noviembre de 2025
download >
Slate Online Training - September 2024 Sessions Day 1
September 2024 - Slate training session Day 1
download >
Slate Online Training - September 2024 Sessions Day 2
September 2024 - Slate training session Day 2
download >
Slate Online Training - September 2024 Sessions Day 3
September 2024 - Slate training session Day 3
download >
Slate Online Training - September 2024 Sessions Day 4
September 2024 - Slate training session Day 4
download >
Slate Online Training - September 2024 Sessions Day 5
September 2024 - Slate training session Day 5
download >
Sesión del día 1 de capacitación en línea de Slate LAR - julio de 2024 (español)
Julio de 2024 Día 1 Sesión
download >
Sesión del día 2 de capacitación en línea de Slate LAR - julio de 2024 (español)
Julio de 2024 Día 2 Sesión
download>
Sesión del día 3 de capacitación en línea de Slate LAR - julio de 2024 (español)
Julio de 2024 Día 3 Sesión
download >
Sesión del día 4 de capacitación en línea de Slate LAR - julio de 2024 (español)
Julio de 2024 Día 4 Sesión
download >
Sesión del día 5 de capacitación en línea de Slate LAR – julio de 2024 (español)
Julio de 2024 Día 5 Sesión
download >
Slate Online Training - June 2023 Sessions Day 1
June 2023 Slate Training Session - Day 1
download >
Slate Online Training - June 2023 Sessions Day 2
June 2023 Slate Training Session - Day 2
download >
Slate Online Training - June 2023 Sessions Day 3
Slate Online Training - June 2023 Sessions Day 3
download >
Slate Online Training - June 2023 Sessions Day 4
Slate Online Training - June 2023 Sessions Day 4
download >
Slate Online Training - June 2023 Sessions Day 5
Slate Online Training - June 2023 Sessions Day 5
download >
Slate Online Training - June 2022 Sessions Day 1
June 2022 - Slate training session Day 1.
download >
Slate Online Training - June 2022 Sessions Day 2
June 2022 - Slate training session Day 2
download >
Slate Online Training - June 2022 Sessions Day 3
June 2022 - Slate training session Day 3
download >
Slate Online Training - June 2022 Sessions Day 4
June 2022 - Slate training session Day 4
download >
Slate Online Training - June 2022 Sessions Day 5
June 2022 - Slate training session Day 5
download >
Slate Online Training - June 2021 Sessions Day 1
June 2021 - Slate training session Day 1.
download >
Slate Online Training - June 2021 Sessions Day 2
June 2021 - Slate training session Day 2
download >
Slate Online Training - June 2021 Sessions Day 3
June 2021 - Slate training session Day 3
download >
Slate Online Training - June 2021 Sessions Day 4
June 2021 - Slate training session Day 4
download >
Slate Online Training - June 2021 Sessions Day 5
June 2021 - Slate training session Day 5
download >